Technical FAQs

Ask a Question

Can the 200A main breaker in a CHOM4284M200GC be replaced with a 100A main breaker?

Issue:
Application

Product Line:
CHOM Load Center

Cause:
Alternate main breaker ampere rating needed

Resolution:
Yes, the factory installed QOM2200VHL could be replaced with an alternate ampere rated QOM2-VHL main breaker. However, the maximum ampere rating of the panel, 200A, cannot be exceeded. 

Was this helpful?
What can we do to improve the information ?