Technical FAQs

Ask a Question

Is the new SCP part number 865-1050-01 compatible with all the XW inverter chargers? (Ex. XW4024, XW6048, XW4548)

865-1050-01 SCP Compatibility
The new part number for the system control panel (SCP) is 865-1050-01.
The XW models had a part number 865-1050 but now the SCP is 865-1050-01 and it is compatible with all XW models.
Was this helpful?
What can we do to improve the information ?