Technical FAQs

Ask a Question

Does the LA400AWK or LA400DS circuit breaker enclosure have knockouts?

Issue:
Product Features

Product Line:
Circuit Breaker Enclosure

Cause:
Clarification of enclosure feature

Resolution:
No, neither the LA400AWK, nor the LA400DS, have any knockouts provided in the enclosure. All conduit entry areas must have field cut openings installed by the installing contractor. 


CTA-ID : 2017101
Was this helpful?
What can we do to improve the information ?