Technical FAQs

Ask a Question

What is the recommended circuit breaker for the ATV31CU22M2 IP54 rated drive?

Issue:
What is the recommended circuit breaker for the ATV31CU22M2 IP54 rated drive?

Product Line:
Altivar ATV31C

Environment:
All

Cause:
Wants to use a circuit breaker on the ATV31CU22M2 drive.

Resolution:
Recommended breakers for the ATV31C........ M2 units are

ATV31C018M2=  GV2L08
ATV31C037M2=  GV2L10
ATV31C055M2=  GV2L14
ATV31C075M2=  GV2L14
ATV31CU11M2=  GV2L16
ATV31CU15M2=  GV2L20
ATV31CU22M2=  GV2L22
 
Was this helpful?
What can we do to improve the information ?