Technical FAQs

Ask a Question

New parameters in the ATV212 V5.4ie53 are not showing in the LCD graphic keypad.

Issue:
It appears that some of the new parameters in the ATV212 V5.4ie53 are not showing in the LCD graphic keypad.
The ATV212 manual says that you need a keypad  V1.1ie29 or later. We have V1.1ie33.

Product Line:
ATV212, S-Flex

Environment:
All

Cause:
Parameters missing labels

Resolution:
The new parameter added on the last ATV212 version are present on the drive and keypad. But they do not have the long label.
So you can configure the drives with these parameters, but you will not have the clear text display.
An evolution request on this subject has been created.
Was this helpful?
What can we do to improve the information ?