Technical FAQs

Ask a Question

How do I set the ATV66 HMI (VW3A66206) to English language?

Issue:
How do I set the ATV66 HMI (VW3A66206)  to English language?

Product Line:
ATV66

Environment:
All
 
Cause:
Installation / Setup

Resolution:
On power up, press the "esc"  3 times to get into programming language mode. Arrow down to English and press enter.

NOTE:  In the US, the ATV66 drive family, including options and accessories like the keypad, were obsoleted in 2004.  Very few repair or replacement parts are still available.
Was this helpful?
What can we do to improve the information ?