Technical FAQs

Ask a Question

What is the rating of XW PDP POS(+) Battery Bus Plate?

Positive battery bus plate can accommodate up to (3) XW+NA Inverter/Chargers, or 250A per inverter for 750ADC max. 
This includes surge capability, so the continuous rating of a (3) inverter (XW+NA6848) system is approx 425ADC.
Was this helpful?
What can we do to improve the information ?