Technical FAQs

Ask a Question

ATV61 Why can I only see the monitoring menu ?

Issue:
ATV61 ATV71 Why can I only see the monitoring menu ?

Product Line:
ATV61 / ATV71

Environment:
All

Cause:
No password protection drive struck in monitoring menu only.

Resolution:
Verify no password protection is set
Verify access level in Main menu
Goto menu 7.3 Display Configuration and verify menu visibility is not restricted.
Was this helpful?
What can we do to improve the information ?