Technical FAQs

Ask a Question

Is the ATV12 series available in panel mount configuration for voltage code F1?

Issue:
Is the ATV12 series available in Panel mount configuration for voltage code F1?
 
Product Line:

ATV12 series drives
 
Environment:

All ATV12 drives with F1 voltage code (120V single phase input, 230V three phase output)
 
Cause:
Information not available in current literature
 
Resolution:
The ATV12P***** series drives are not available with voltage code F1 for single phase 120VAC INPUT and 230V 3 phase Output.
Was this helpful?
What can we do to improve the information ?