Technical FAQs

Ask a Question

What wire size can I use on the Telefast ABE7 blocks

Issue:
What wire size can I use on the Telefast ABE7 blocks

Product Line:
Telefast ABE7

Resolution:
The follwoing wire sizes can be used with the Telefast ABE7 blocks.
Stranded: 26 to 14 awg (1 wire)
Stranded with cable end: 28 - 16 awg (1 wire), 28 - 20 (2 wire)
Solid Wire:  26 - 12 awg (1 wire), 24 - 14 (2 wire)
Was this helpful?
What can we do to improve the information ?