Technical FAQs

Ask a Question

What is the maximum number of operators allowed in the door of the LE1D enclosed D-Line units?

Issue:
What is the maximum number of operators allowed in the door of the LE1D enclosed D-Line units?

Product Line:
LE1D Enclosed D-Line

Environment:
All Product Lines

Cause:
The product selector will not let me select a start/stop, and 2 pilot lights

Resolution:
The maximum number of operators is 3.

Start/Stop is considered 2 operators.
Was this helpful?
What can we do to improve the information ?