Technical FAQs

Ask a Question

Can I control the speed on two Altivar drives with one potentiometer?

Issue:
Can I control the speed on 2 Altivar drives with one potentiometer?

Product Line:
Altivar drives

Environment:
All

Cause:
N/A

Resolution:
Yes, one potentiometer is capable of serving as the speed reference for drives. As long as minimum and maximum voltage reference is available each analog input.
Was this helpful?
What can we do to improve the information ?