Technical FAQs

Ask a Question

What is the torque requirement for the mounting nuts used to secure the lugs provided in the QOL125 and QOL3125 Main Lug Kits to the load center busbars?

Issue:
Specifications

Product Line:
Load Center Accessory

Cause:
Torque requirements

Resolution:
The lug mounting nuts should be torqued to 75 Lb-In (8.5 N-m)
Was this helpful?
What can we do to improve the information ?