Technical FAQs

Ask a Question

Can you use the M221 PLC's TMH2GDB keypad display on the ATV630 process drive?

Issue:
Can you use the M221 PLC's TMH2GDB keypad display on the ATV630 process drive?

Product Line:
Altivar ATV630

Environment:
All ATV630 drives

Cause:
Wants to know if the TMH2GD8 keypads will work on the ATV630 drives?

Resolution:
No the TMH2GDB keypad will not work on the ATV630 or any of the ATV drives.
The hardware is the same  as the VW3A1111 keypad but the firmware is not.  The firmware can not be updated either.
 
Was this helpful?
What can we do to improve the information ?