Technical FAQs

Ask a Question

What is the AIR of JJ breakers?

Product Line:
Circuit Breakers 

For Powerpact J Frame Circuit Breakers, the JJ version has the following AIR: 
100 kA @240 Vac
65 kA @ 480 Vac
25 kA @ 600 Vac
Was this helpful?
What can we do to improve the information ?