Technical FAQs

Ask a Question

Why does my Conext SW draw from the grid when Load Shaving?

To minimize draw from the grid during non-solar hours, set Load Shave Amps to "0". 
Make sure loads are fairly well balanced between L1 and L2 when powering 120VAC loads. 
Was this helpful?
What can we do to improve the information ?