Technical FAQs

Ask a Question

Knurled Screw on Combination Starters

Issue:
What is the part number for the knurled screw on the front of a combination starter?

Product Line:
NEMA Combination Starters - GIC Product

Environment:
US Product

Cause:
Product Characteristics

Resolution:
The knurled screw on the face of NEMA combination starters size 0 through 4 is 30007-28201, the replacement washers for this screw are 153-D15-X22, and the nut with retaining bracket is 23502-20003.
Was this helpful?
What can we do to improve the information ?