Technical FAQs

Ask a Question

Will our Ethernet IP VW3A3316 option card support the AB SLC505 using C triple P or UDP protocol?

Issue:
Will our Ethernet IP VW3A3316 option card support the AB SLC505 using C triple P or UDP protocol?

Product Line:
Altivar ATV61 with VW3A3316 option card.

Environment:
All

Cause:
Wants to know if our Ethernet VW3A3316 card supports udp and c triple P protocol.

Resolution:
No, our Ethernet IP option card do not support either upd or c triple P.

 
Was this helpful?
What can we do to improve the information ?