Technical FAQs

Ask a Question

Can you put the E-flex enclosed drive inside of an NEMA 4X enclosure?

Issue:
ATV61 in a E-Flex enclosure- customer wants to put the entire E-Flex in another enclosure (Nema 4X enclosure)
 
Product Line:
ATV61 drives in E-Flex enclosure
 
Environment:
E-Flex enclosures
 
Cause:
Install the E-Flex in a Nema 4X enclosure
 
Resolution:
We cannot recommend this because we have not tested this and their could be heating issues with doing this.
 



 
Was this helpful?
What can we do to improve the information ?