Technical FAQs

Ask a Question

What size screw is used to hold in the 9080LB Type covers on the 9080LBA Type power distribution blocks?

Issue:
What size screw is used to hold in the 9080LB Type covers on the 9080LBA Type power distribution blocks?

Product Line:
9080 Power Distribution Blocks

Environment:
US Product Lines

Cause:
Can not find it in the Digest

Resolution:
Screw size is #4-40 x .375"
 
Was this helpful?
What can we do to improve the information ?