Technical FAQs

Ask a Question

How high / tall is the 400A NQ main lug dead front trim p/n 80122-056-03?

Issue:
How high / tall is the 400A NQ main lug dead front trim  p/n 80122-056-03?

Product Line:
NQ Panelboards

Environment:
Installation

Cause:
Gaps with wrong Deadfront shipped

Resolution:
The Main Lug dead front Trim should be 8.58" H 
Was this helpful?
What can we do to improve the information ?