Technical FAQs

Ask a Question

Where is the 0V terminal on the ATV32 shown in the manual?

Issue:
Trying to connect external 24VDC

Product line:
Altivar 32, ATV32

Environment:
All models

Cause:
Error in the published manuals.

Resolution:
There is no 0V terminal  Use a COM terminal for a negative side of the external 24VDC supply.
Was this helpful?
What can we do to improve the information ?