Technical FAQs

Ask a Question

Is there a conversion kit to convert an ATV66 that was custom enclosed over to a ATV61/71 drive?

Issue:
Is there a conversion kit to convert an ATV66 that was custom enclosed over to a ATV61/71 drive?

Product Line:
ALTIVAR 61, ALTIVAR 71

Environment:
All

Cause:
ATV66 to an ATV61/ATV71 conversion

Resolution:
No, there is not a retro kit to convert over an existing enclosed ATV66 to a ATV61 or ATV71.  If the customer decides to convert the drive over they will be responsible for their own conversion and modifications to the existing enclosure.
 
Was this helpful?
What can we do to improve the information ?