Technical FAQs

Ask a Question

ATV18 drive has a run command but it is not outputing any voltage to the motor.

Issue:
ATV18 drive has a run command but it is not outputing any voltage to the motor.

Product Line:
 Altivar  ATV18

Environment:
All

Cause:
Drive appears to be running it shows 30hz on the display but the motor is not turning.

Resolution: 
First make sure your motor is connected to the drive.
Get a meter and check the output voltage on T1 T2 T3 of the drive to see if the drive is outputing any voltages.
Try resetting the drive back to a factory default to see if the drive can be reset.
If there is still no output, would need tor eplace the drive.
Was this helpful?
What can we do to improve the information ?