Technical FAQs

Ask a Question

What is the degree of protection for the 9050JCK Type timers?

Issue:
What kind of environment are the 9050JCKs rated for?

Product Line:
9050 Type JCK Timers

Environment:
US Product Lines

Cause:
Can not find it in the Digest

Resolution:
These relays have a IP20 rating. IP20 is protection against solid objects greater than 12mm, and no protection against liquids.
Was this helpful?
What can we do to improve the information ?