Technical FAQs

Ask a Question

Can you use the Apogee P1 VW3A3314 card on the ATV71 drives?

Issue:
Can you use the Apogee P1 VW3A3314 card on the ATV71 drives?

Product Line:
Altivar ATV71

Environment:
All

Cause:
Wants to use the VW3A3314 option card on the ATV71 drives.

Resolution: 
The VW3A3314 Apogee P1 option card is only available to be used on the ATV61 only.  You can not use this card on the ATV71 drives.
Was this helpful?
What can we do to improve the information ?