Technical FAQs

Ask a Question

Can you put an Illuminated push button to 9001KZC297?

Issue: 
Can you put an Illuminated push button to 9001KZC297?

Product Line:
Control Stations

Environment:
30mm Push Buttons and Control Stations

Resolution:
No. The light module will not fit because the spring of the lock occupies one side of the back of the push button assembly, a light module will occupy both sides.
Even with the use of a shallow depth light module, since it doesn't have a translating pin, you cannot actuate a contact block behind it.

 
Was this helpful?
What can we do to improve the information ?