Technical FAQs

Ask a Question

Can I change the default parameter displayed by my ATS48, from the remote keypad?

Issue:
 Can I change the default parameter displayed by my ATS48, from the remote keypad?
 
Product line:
ATS48 soft starts
 
Environment:
Units equipped with remote mount keypad kit
 
Cause:
Customer is attempting to change the default value via the remote keypad but it is not changing.
 
Resoultion:
The default value displayed by the display can only be changed on the Soft Starter itself.  It can not be changed from the remote keypad.  Once changed on the ATS48, it will display the new value on the Soft Starter and remote display both, but it can only be changed from the face of the ATS48.




 
Was this helpful?
What can we do to improve the information ?