Technical FAQs

Ask a Question

What is the accuracy of the analog input of Altivar 32 drive

Issue:
Accuracy of analog input

Product:
Altivar 32

Environment:
All models and serial numbers
 
Cause:
None

Resolution:
The accuracy of the analog inputs is +/- 0.6% for a temperature variation of 60 deg C
 
Was this helpful?
What can we do to improve the information ?