Technical FAQs

Ask a Question

Interface Modules for NEMA Starters and Contactors

Issue:
Is there an interface module for the NEMA contactors and Starters so that the coil can be energized from a PLC or similar device?

Product Line:
NEMA Contactors and Starters - GIC Product

Environment:
US Product

Cause:
Product Application and Integration

Resolution:
There is no dedicated interface module for these units.  The easiest way to accomplish this type of control is to install an interposing relay (such as an ice cube type).  The PLC could energize the relay which would in turn pick up the coil.
Was this helpful?
What can we do to improve the information ?