Technical FAQs

Ask a Question

CHOM4284M2100GC: Can this be upgraded to a 200A Main Breaker Load Center?

Issue:
Product Features

Product Line:
Canadian HOMELINE CHOM

Cause:
Clarifying product feature

Resolution:
Yes, the labeling is marked for a 200A maximum main. The factory installed QOM2100VHL could be removed and replaced with a QOM2200VHL main breaker kit.
Was this helpful?
What can we do to improve the information ?