Technical FAQs

Ask a Question

2510K Date Codes

Issue:
Where is the date code on 2510K switches and how is it interpreted?

Product Line:
2510K NEMA Switches - GIC Product

Environment:
US Product

Cause:
Product Characteristics

Resolution:
The date code is located on the side of the switch itself underneath the IEC stamping.  It is a four digit number in the form YYWW.  YY is the two digit year of manufacture.  WW is the numbered week of that year referenced.
Was this helpful?
What can we do to improve the information ?