Technical FAQs

Ask a Question

Can more than one Display parameter be shown on ATV312 Remote keypad?

Issue:
Can more than one Display parameter be shown on ATV312 Remote keypad?
 
Product Line:
ATV312
 
Environment:
All
 
Cause:
Customer wants to display more than one display parameters.

Resolution:
The ATV312 Remote keypad can only show one display parameters at a time.
Was this helpful?
What can we do to improve the information ?