Technical FAQs

Ask a Question

Do any parameters in a drive need to be changed when using a DV/DT filter?

Issue:
Do any parameters in a drive need to be changed when using a DV/DT filter? 
 
Product Line:
All Altivar drives.
 
Environment:
All serial numbers:
 
Cause:
Information not available in current literature.
 
Resolution:
No, there are no parameters that need to be changed from factory default when using a DV/DT filter on the output of the drive.   On the ATV61 and ATV71 series drives, the "Sinus Filter" parameter does need to be changed if a true Sinus filter is being used, but not when using a DV/DT filter.
 







 
Was this helpful?
What can we do to improve the information ?