Technical FAQs

Ask a Question

What are the dimensions for the J250AWK and J250AWKVW circuit breaker enclosures?

Issue:
Dimensions

Product Line:
Circuit Breaker Enclosure

Cause:
Dimensions

Resolution:
These enclosures are 32.26" H x 9.72" W x 5.61" D.

Click this link to access the Approval Drawing #3363S:
http://static.schneider-electric.us/docs/Circuit%20Protection/Circuit%20Breaker%20Enclosures/3363S.pdf

The drawing is also attached. 


CTA-ID : 2049174
Was this helpful?
What can we do to improve the information ?