Technical FAQs

Ask a Question

Can the XW+NA AUX port be set to trigger on time?

Issue:
Can the XW+NA AUX port be set to trigger on time?

Product Line:
Conext XW+ Series

Environment:
Conext SCP or ComBox

Cause:
AUX trigger was recently added to XW+ systems

Resolution:
Yes, TimeOfDay is now an available trigger for the AUX output. While it is set to Automatic with this trigger, the AUX output will be active by default, and a trigger block period can be set, during which the AUX output will become inactive.

For example, with the following settings:
Active Level: ActiveHigh
Trig Block Start: 12:00PM
Trig Block Stop: 3:00PM

The AUX output will produce 12V at all times except for the period from 12-3PM, during which it will be inactive.
Was this helpful?
What can we do to improve the information ?