Technical FAQs

Ask a Question

Where can I find information on the input line current for the ATV61 drives?

Issue:
Where can I find information on the input line current for the ATV61 drives?

Product Line:
ATV61/71

Environment:
All serial numbers for ATV61/71

Cause:
Wants to know what the input line current is.

Resolution:
Information for the line current for the ATV61 drive can be found in the ATV61 installation manual
 
Was this helpful?
What can we do to improve the information ?