Technical FAQs

Ask a Question

Are the printed circuit boards in the ATV212 drive conformal coated?

Issue:
Conformal coating of the pc boards in the ATV212

Product Line:
Altivar 212
 
Environment:
All models and serial numbers
 
Cause:
None
 
Resolution:
Yes, but not on the bus bars. You still have to watch out for corrosive gases.   
 
Was this helpful?
What can we do to improve the information ?