Technical FAQs

Ask a Question

How can I field wire a damper circuit in an E-flex enclosure drive system?

Issue:
How can I field wire a Damper Circuit in an E-Flex enclosure system?

Product Line:
E-Flex

Environment:
All serial numbers for E-Flex

Cause:
N/A

Resolution:
Remove jumper from 6 and 6A on field terminal block
Replace with Damper end of close switch on 6 and 6A
Wire in Damper solenoid on 6A and 24 (ground)
Wire in auto start contact on 6a and 7
The wiring example below was taking out of the enclosed Econoflex 58 manual but it can be used on the new E-flex and other enclosed drives that have the same RCR control wiring.


 
Was this helpful?
What can we do to improve the information ?