Technical FAQs

Ask a Question

What are the part number for the replacement deadfronts for an NQ418L1C14?

Issue: 
What are the part number for the replacement deadfronts for an NQ418L1C14?

Product Line
NQ 14"W Panelboards

Environment: 
Maintenance

Cause: 
Replacement

Resolution:
Part numbers for the deadfronts are : 

Branch breaker deadfront 80122-478-01
Main Lug deadfront 80122-479-01 
Bottom deadfront 80122-479-02 

*Note*
Part numbers will need to be quoted thru Local Distributor, or SQ D/SE Sales Office and order forced onto the Peru Mfg Plant

 
Was this helpful?
What can we do to improve the information ?