Technical FAQs

Ask a Question

Can you connect 24vdc or 120vac to the start terminals 5-6 on the S-flex enclosed drive?

Issue:
Can you connect 24vdc or 120vac to the start terminals 5-6 on the S-flex enclosed drive?

Product Line:
Altivar ATV21 or ATV212 S-flex enclosed

Environment:
All

Cause:
They have a start command with voltage and want to know if they can put it on the start terminals 5-6.

Resolution:
We only recommend that you put a dry contact between terminals 5-6 for the start command.  We are supplying the 120vac power to these terminals.  Please do not bring your own voltage into there terminals.
Was this helpful?
What can we do to improve the information ?