Technical FAQs

Ask a Question

Is there a Certificate of Orign for Altivar AC Drives or Altistart Softstarts

Issue: 
Certificate of Orign for Altivar AC Drives or Altistart Softstarts

Product Line: 
All Drives and Soft starts

Environment: 
All Drives and Soft Starts

 Resolution: 
Per PLE, if a request is regarding specific part number(s) I may be able to obtain the Certificate, however different part numbers and frame sizes are manufactured in different locations.  Unfortunately, for that reason, there is no single certificate for any product range, like Altivar 61, of the AC Drives and Softstarts. 
 
Was this helpful?
What can we do to improve the information ?