Technical FAQs

Ask a Question

What BACnet point do I use to tell if the E-Flex is in hand or auto?

Issue:
BACnet reading digital input
 
Product Line:
ATV61/ATV71
 
Environment:
All models and serial numbers
 BACnet option card VW3A3315
 
Cause:
None
 
Resolution:
Binary input #8 - DI3 ACT 
 
Was this helpful?
What can we do to improve the information ?