Technical FAQs

Ask a Question

Can the ATS48 softstarter be configured to continue running even after it loses the modbus communications network?

Issue:
Can I get the ATS48 softstarter to keep running even after it loses communications?

Product Line:
ATS48

Environment:
All serial numbers for ATS48

Cause:
N/A

Resolution:
No, there is no way to disable the Modbus timeout on the softstarter. It ranges from 0.1s to 60s.
 
Was this helpful?
What can we do to improve the information ?