Technical FAQs

Ask a Question

Is there an exchange program for the Altistart 22?

Is there an exchange program for the Altistart 22?
Issue: 
Is there an exchange program for the Altistart 22?
 
Product Line:
ATS22
 
Environment:
All serial numbers
 
Cause:
N/A
 
Resolution:
No, Schneider do not offer an exchange program for the Altistart 22.
Was this helpful?
What can we do to improve the information ?