Technical FAQs

Ask a Question

Can I connect multiple drives of different part numbers to a single VW3A1101 HMI?

Issue:
Can I connect multiple drives of different part numbers to a single VW3A1101 HMI?

Product Line:
ATV61, ATV71, ATV32, ATV312, ATV212.

Environment:
All models with a firmware revision capable of supporting the VW3A1101 keypad.

Cause:
Information not available in current literature.

Resolution:
No, it is not possible to connect multiple drives of different part numbers, to a single HMI.   On the ATV61 and ATV71 series drives, it is possible to connect multiple drives to a single HMI, but you can not mix drive part numbers.   You can not connect to ATV61 and ATV71 drives, with the same HMI.
Was this helpful?
What can we do to improve the information ?