Technical FAQs

Ask a Question

Where can I find programming assistance setting up the Apogee P1 card on the ATV21 drive?

Issue:
Where can I find programming assistance setting up the Apogee P1 card on the ATV21 drive?

Product Line:
Altivar ATV21 and SFD21 with optional Apogee P1 card.

Environment:
All

Cause:
Needs programming assistance setting up the Apogee P1 card on the ATV21 drive.

Resolution:
F829=3 for Apogee P1
F890= address 1 or you choose
F891= baud rate choose
F892= communication timeout fault 100 or 10 seconds