Technical FAQs

Ask a Question

Where would you wire the output filter or load reactor on a enclosed package drive with a bypass option?

Issue:
Where would you wire the output filter or load reactor on a enclosed package drive with a bypass option?

Product Line:
E-Flex, M-Flex, MCC or any enclosed drive with a bypass option.

Environment:
All

Cause:
They want to add an output filter to their drive but they have a full voltage bypass option.

Resolution:
You can wire the output filter between the Drives U, V and W terminals and the output contactors L1 L2 L3 terminals.
Was this helpful?
What can we do to improve the information ?