Technical FAQs

Ask a Question

Are there any known issues controlling an ATV312 series drive with an Allen Bradley Slick 500 controller?

Issue:
Are there any known issues controlling an ATV312 series drive with an Allen Bradley Slick 500 controller?

Product Line:
ATV312 series drives

Environment:
Systems in which an Allen Bradley Slick 500 controller is being used to control the drive.

Cause:
General inquiry before purchase

Resolution:
The ATV312 can be controlled by the Slick 500 controller, but implicit messaging must  be used.  The com scanner can not be used in this configuration.
Was this helpful?
What can we do to improve the information ?