Technical FAQs

Ask a Question

Will GFCI's work on a variable frequency drive?

Issue:
Updated Ground Fault Circuit Interrupters and variable frequency drives.

Product Line:
Altivar Variable Frequency Drives

Environment:
All models and serial numbers

Cause:
Most GFCI will not work on a drive because of high frequency noise. Need a special GFI that is immune from noise.

Resolution:
It is not recommend by Schnieder Electric, however, there is a company called Bender that can provide these.  http://www.bender.org/
 
Was this helpful?
What can we do to improve the information ?